IMX8M-EVK & NXP OLED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M-EVK & NXP OLED

4,288 Views
oli1
Contributor II

Hi,

We recently purchased the NXP MIPI-DSI OLED for use with our IMX8M-EVK board but we're unable to get the panel to display anything.

I have made sure the correct device tree is used (I've both explicitly set this in the configs & set on boot via u-boot cmd), I'm using the fsl-imx8mq-evk-dcss-rm67191.dts tree.

This is the error I see in the bootlogs.

[1.054926] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)
[1.062412] nwl_dsi-imx mipi_dsi@30A00000: Using DCSS as input source
[1.069107] imx-drm display-subsystem: failed to bind mipi_dsi@30A00000 (ops imx_nwl_dsi_component_ops): -19
[1.079031] imx-drm display-subsystem: master bind failed: -19

Any help with this would be greatly appreciated.

Kind regards

Oli

Tags (2)
0 Kudos
Reply
4 Replies

3,273 Views
RonIovine
Contributor I

I am also seeing the same mipi bind error and also cannot access this document/link, is there anyone @nxp that can help with this, original post is almost 3 years old, is anyone there @nxp???

0 Kudos
Reply

3,790 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Oliver,
You could take a look to the following Community document for additional related information:
https://community.nxp.com/docs/DOC-342431


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

3,791 Views
westbrook
Contributor III

Hi Carlos,

I can not access this link:

https://community.nxp.com/docs/DOC-342431

Can you share me the content of this link. I am also facing the oled issue.

Thank you.

Best Regards,

Xiao

3,478 Views
amberworth
Contributor III

I'm having the same issue. Getting Access denied when trying to access the document.

0 Kudos
Reply