IMX8EVK HDMI display example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8EVK HDMI display example

6,836件の閲覧回数
lingguan
Contributor II

Hello,

     I want to ask whether there are some examples to test imx8mqevk HDMI ? For example, showing some pictures or videos, or QT demo ?

Sincerely.

ラベル(1)
0 件の賞賛
返信
11 返答(返信)

6,477件の閲覧回数
pavel_badin
Contributor I

Hello,

probably might be funny reason but on MEK CPU board there is no HDMI signal if the mouse/keyboard are not plugged into the USB connector. Just make sure it is not this reason :smileyhappy:

0 件の賞賛
返信

6,477件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

the default demo image supports HDMI directly, you can use mfgtool to download demo image to board then boot up, you can play video or somthing to the HDMI directly

0 件の賞賛
返信

6,477件の閲覧回数
lingguan
Contributor II

Hi Joan Xie,

    If I stop uboot, there are something displayed on the HDMI display. But when I start the linux, it's "no signal" on the display.

   I use the image L4.9.51 and bitbake fsl-image-qt5-validation-imx-xwayland.

0 件の賞賛
返信

6,477件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you don't stop the uboot, the board can boot up successfully?

0 件の賞賛
返信

6,477件の閲覧回数
lingguan
Contributor II

pastedImage_1.png

0 件の賞賛
返信

6,476件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

have you fixed the issue?

0 件の賞賛
返信

6,477件の閲覧回数
lingguan
Contributor II

Dear Xie,

      No, I cannot solve the problem. I also try the 4.9.123 kernel, but no HDMI signal.

Sincerely.

0 件の賞賛
返信

6,477件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I haven't tested this version, but when I use UUU tool to program the newer yocto version, the image supports HDMI output as default

0 件の賞賛
返信

6,477件の閲覧回数
lingguan
Contributor II

What is the yocto version? And what is the kernel version?

Thank you.

0 件の賞賛
返信

6,477件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yocto 4.14.98

0 件の賞賛
返信

6,477件の閲覧回数
lingguan
Contributor II

yeah, the board can auto boot up successfully.

0 件の賞賛
返信