IMX8EVK HDMI display example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8EVK HDMI display example

6,744 次查看
lingguan
Contributor II

Hello,

     I want to ask whether there are some examples to test imx8mqevk HDMI ? For example, showing some pictures or videos, or QT demo ?

Sincerely.

标签 (1)
0 项奖励
回复
11 回复数

6,385 次查看
pavel_badin
Contributor I

Hello,

probably might be funny reason but on MEK CPU board there is no HDMI signal if the mouse/keyboard are not plugged into the USB connector. Just make sure it is not this reason :smileyhappy:

0 项奖励
回复

6,385 次查看
joanxie
NXP TechSupport
NXP TechSupport

the default demo image supports HDMI directly, you can use mfgtool to download demo image to board then boot up, you can play video or somthing to the HDMI directly

0 项奖励
回复

6,385 次查看
lingguan
Contributor II

Hi Joan Xie,

    If I stop uboot, there are something displayed on the HDMI display. But when I start the linux, it's "no signal" on the display.

   I use the image L4.9.51 and bitbake fsl-image-qt5-validation-imx-xwayland.

0 项奖励
回复

6,385 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you don't stop the uboot, the board can boot up successfully?

0 项奖励
回复

6,385 次查看
lingguan
Contributor II

pastedImage_1.png

0 项奖励
回复

6,384 次查看
joanxie
NXP TechSupport
NXP TechSupport

have you fixed the issue?

0 项奖励
回复

6,385 次查看
lingguan
Contributor II

Dear Xie,

      No, I cannot solve the problem. I also try the 4.9.123 kernel, but no HDMI signal.

Sincerely.

0 项奖励
回复

6,385 次查看
joanxie
NXP TechSupport
NXP TechSupport

I haven't tested this version, but when I use UUU tool to program the newer yocto version, the image supports HDMI output as default

0 项奖励
回复

6,385 次查看
lingguan
Contributor II

What is the yocto version? And what is the kernel version?

Thank you.

0 项奖励
回复

6,385 次查看
joanxie
NXP TechSupport
NXP TechSupport

yocto 4.14.98

0 项奖励
回复

6,385 次查看
lingguan
Contributor II

yeah, the board can auto boot up successfully.

0 项奖励
回复