IMX8DXL(Silicon b0) SCFW build Error (imx-scfw-porting-kit-1.13.0.tar.gz)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8DXL(Silicon b0) SCFW build Error (imx-scfw-porting-kit-1.13.0.tar.gz)

1,616 次查看
eric9
Contributor I

Hello,

I am trying to build scfw for IMX8DXL (silicon b0)

I got the latest version (imx-scfw-porting-kit-1.13.0.tar.gz) from NXP web site.

1.

When installing scfw-porting kit, I can't find out porting kit for mx8dxl_b0

eric9_1-1661397427566.png

There are only mx8qx_b0 and mx8dxl_a0....

Could I use mx8qx_b0 and mx8dxl_a0 instead of mx8dxl_b0?

 

2.

I tried to build using scfw_export_mx8qx_b0.tar.gz...

According to guide, I installed toolchain for that (version 8-2018-q4)

eric9_0-1661397317254.png

When make....I encountered build error like below...

eric9_3-1661397714188.png

eric9_2-1661397699276.png

(scfw_export_mx8dxl_a0.tar.gz...have same issue too..)

Pls let me know the solution...

 

 

 

0 项奖励
回复
3 回复数

1,473 次查看
GaneshaKulal
Contributor I

Hello, 

Where I should get SCFW for SXL/DXL controller? Please share the link.

0 项奖励
回复

1,583 次查看
justin_jiang
NXP Employee
NXP Employee

2. Please don't use 8qx package to build 8dxl, there is no prebuilt binaryies. Please use 8dxl a0 package. 

 

0 项奖励
回复

1,584 次查看
justin_jiang
NXP Employee
NXP Employee

1. Please check the release note in the package,

 Support added for i.MX8DXL B0. i.MX8DXL A1 and B0 use the same code so the only source tarball is for A0.

  Also, binaries created for i.MX8DXL are run-time compatible to both silicon versions so always build with R=A0.

justin_jiang_0-1662632699663.png

 

0 项奖励
回复