【IMX8DXL】HSM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,730件の閲覧回数
jianwei_lan
Contributor III

Dear friend

I am evaluating i.MX8DXL + Yocto L5.4.78_2.3.0.

1)Does i.MX8DXL have HSM modue?

2)How to use HSM module? It have any demo provide?

----------

BR,

0 件の賞賛
返信
1 解決策
1,724件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, imx8DXL includes HSM, if you mean hardware secure module, for more detailed information, you can refer to the:

https://source.codeaurora.org/external/imxsupport/imx_sec_apps/tree/hsm_she_examples

you also can refer to the readme of this link

元の投稿で解決策を見る

1 返信
1,725件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, imx8DXL includes HSM, if you mean hardware secure module, for more detailed information, you can refer to the:

https://source.codeaurora.org/external/imxsupport/imx_sec_apps/tree/hsm_she_examples

you also can refer to the readme of this link