IMX8 issue】

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 issue】

1,765 Views
gravity_one
Contributor III

hello,

i use mcimx8-8x-bb ,linux kernel is started,USB connection is normal with USB flash drive,and can read data。

but connect to the computer, the computer(win10) does not have any prompt.

usb cable is fine,because it connect debug is ok,can print info。

0 Kudos
Reply
3 Replies

1,693 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

If you are use theMCIMX8QXP-CPU CPU board, here you need to change the boot mode to download mode, then you can see the board detect when you connect your board to PC.

0 Kudos
Reply

1,693 Views
gravity_one
Contributor III

mirco USB can download image with UUU tools?

switch :serial mode,but mirco USB connect PC ,PC no detect device。

i use type-C can download image with UUU tools。

0 Kudos
Reply

1,693 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The Micro USB for UART debug not download images. USB-OTG is for downloading. Yes, type-C can download image with UUU tools.

0 Kudos
Reply