IMX8 Switching Processors and the Change in Firmware/Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 Switching Processors and the Change in Firmware/Software

Jump to solution
3,896 Views
Phoenix42
Contributor II

Hey y'all,

We're having some internal trouble and realized there may be a need to switch from the I.mx 8M mini to a more powerful chip in the I.MX 8 family (we have yet to decide what chip). Currently we are working with the NXP 8M-mini eval kits using quite a few peripherals and the Android OS. 

Should we expect there to be a major software/firmware rework due to the switch in processors, or will it be minor changes such as downloading a few build/image files and moving various connections? Originally, I noticed that the SDK seem uniform across NXP devices, but I didn't want to ruin our team based on one assumption.

I am inexperienced in these matters and NXP devices so I'd appreciate any guidance. 

0 Kudos
Reply
1 Solution
3,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi Connor

 

>Should we expect there to be a major software/firmware rework due to the switch in processors, or will it be >minor changes such as downloading a few build/image files and moving various connections?

 

yes changes are significant. i.MX8(X) series use SCFW concept for programming:

https://imxdev.gitlab.io/tutorial/System_controller_unit_introduction_for_imx_8qxp_mek/

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

 

Best regards
igor

View solution in original post

0 Kudos
Reply
5 Replies
3,892 Views
igorpadykov
NXP Employee
NXP Employee

Hi Connor

 

>Should we expect there to be a major software/firmware rework due to the switch in processors, or will it be >minor changes such as downloading a few build/image files and moving various connections?

 

yes changes are significant. i.MX8(X) series use SCFW concept for programming:

https://imxdev.gitlab.io/tutorial/System_controller_unit_introduction_for_imx_8qxp_mek/

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

 

Best regards
igor

0 Kudos
Reply
3,844 Views
Phoenix42
Contributor II

Igor,

The SCFW download is under the Linux download page so I'm a bit confused as to its purpose in Android. Previously, since we were working off the Demos provided in the SDK, I was under the belief that the SDK download was enough. Thus from there we would simply replace the surrounding libraries and some references.

Just to confirm if I am understanding this right, we would need to restart development as the SCFW is different for every chip in the I.Mx 8 Family and there is no consistency between the chips. The SCFW is also separate to the SDK that NXP provides and is another layer/download that needs to be managed.

0 Kudos
Reply
3,826 Views
igorpadykov
NXP Employee
NXP Employee

Hi Connor

 

Android is based on linux so SCFW is used for i.MX8(X) development too.

i.MX8M Mini has not SCFW.

 

Best regards
igor

0 Kudos
Reply
3,803 Views
Phoenix42
Contributor II

So wait, there is no SCFW for the 8M-Mini, but there is a required SCFW for the rest of the I.mx 8 series? So if we switched to the 8M-plus there would be a SCFW. Or is that only for the ones with an 8X? 

You seem to contradict yourself here by saying that the I.mx 8 series require SCFW, and then say separately that the 8M-mini does not.

0 Kudos
Reply
3,795 Views
igorpadykov
NXP Employee
NXP Employee

>there is no SCFW for the 8M-Mini, but there is a required SCFW for the rest of the I.mx 8 series?

 

SCFW is used only for i.MX8QXP, i.MX8QM:

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

1.jpg

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

2.jpg

 

 

i.MX8M Mini, Plus do not use SCFW.

 

Best regards
igor

0 Kudos
Reply