IMX8 MIPI CSI PHY CLOCK-Max frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 MIPI CSI PHY CLOCK-Max frequency

2,264 Views
james_kim
Contributor II

Hi,

I'm working on MIPI CSI camera. My camera is sending mipi clock rate at 750 MHz. IMX8 EVK could not receive mipi data completely, there are some missing pixels. My setting is Phy clock at 333 MHz. With same setting in NXP, I reduce mipi clock to 350 MHz. Everything is working good. What is the maximum CSI PHY clock frequency?

Regards,

James 

1 Reply

2,108 Views
b36401
NXP Employee
NXP Employee

MIPI CSI controller by itself supports up to 1.5Gbps per lane.

0 Kudos
Reply