IMX8 MIPI CSI PHY CLOCK-Max frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 MIPI CSI PHY CLOCK-Max frequency

1,771件の閲覧回数
james_kim
Contributor II

Hi,

I'm working on MIPI CSI camera. My camera is sending mipi clock rate at 750 MHz. IMX8 EVK could not receive mipi data completely, there are some missing pixels. My setting is Phy clock at 333 MHz. With same setting in NXP, I reduce mipi clock to 350 MHz. Everything is working good. What is the maximum CSI PHY clock frequency?

Regards,

James 

ラベル(1)
1 返信

1,615件の閲覧回数
b36401
NXP Employee
NXP Employee

MIPI CSI controller by itself supports up to 1.5Gbps per lane.

0 件の賞賛
返信