IMX8: How to partition display for two OS in custom image of imx8mqevk with jailhouse hypervisor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8: How to partition display for two OS in custom image of imx8mqevk with jailhouse hypervisor

1,881 次查看
vsuneja63
Contributor III

Hi, 

Thanks!

Using jailhouse hypervisor to load two custom images in imx8mqevk. Not getting any breakthrough to display the second image of non-root cell. Can you help on the scenario or steps for partitioning the same display screen for both images? 

标签 (1)
0 项奖励
回复
5 回复数

1,857 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the imx8mqevk or imx8qmevk board? Which version BSP are you using?

0 项奖励
回复

1,841 次查看
vsuneja63
Contributor III

Hi,

Thanks!

Any suggestions on the same?

0 项奖励
回复

1,851 次查看
vsuneja63
Contributor III

Hi,


Thanks!


I am using IMX8MQ EVK. BSP 5.4.51

0 项奖励
回复

1,826 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I do not found the official released BSP you are used 5.4.51.  As we do not have the example or document for your need, here I found the code and  i.MX Virtualization User's Guide document do help for you:

https://source.codeaurora.org/external/imx/linux-imx/commit/?id=1afdd5020d49f76912aff596418a7f343cea...

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true

 

 

0 项奖励
回复

1,753 次查看
vsuneja63
Contributor III

Hi,

Thanks!

Does steps available for 5.4.24 bsp to partition display for two OS. Can you suggest more info on the same? I could see jailhouse primary root cell Linux UI is up but not getting how to make non-root cell Linux UI up. Is there any way other than partitioning of display, possible to achieve by using two display screen? 

0 项奖励
回复