IMX8 Boot failure from SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 Boot failure from SD

1,779件の閲覧回数
hangfang_zhang
Contributor I

Hi, 

I have an MCIMX8M Quad EVK (2017 REV) and have built an image for it, which can be loaded to SD card and run on this board properly after setting right boot mode.

I recently bought several new MCIMX8M Quad EVKB (2018 REV), which I thought should be able to share the same image. However, it failed to boot with the old image on new boards I bought.

Anyone knows the difference of the two REVs of IMX8? Do I need to set different MACHINE for two boards when building Yocto? Currently what I set is "MACHINE= imx8mqevk".

Thanks,

Hannah

0 件の賞賛
返信
2 返答(返信)

1,682件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

That was probably your board have an old silicon revision. In this case, the newest BSP will not work with the old board and vice versa. For the new i.MX8MQ that you have recently bought, I suggest you use our newest BSP. They should work without any problem.

Best regards,

Diego.

1,682件の閲覧回数
hangfang_zhang
Contributor I

Hi Diego,

Thank you. I tried your advice to build with newest BSP and the image works properly. I shouldn't stick on the old BSP. Thank you so much.

Thanks,

Hannah

0 件の賞賛
返信