IMX7ULP : .sdcard file flashing on SDcard : Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX7ULP : .sdcard file flashing on SDcard : Error

3,017 次查看
chum
Contributor III

vanessamaegima

imx7ulp‌.sdcard dual_boot‌ arm cortex-a7 #arm-cortex-m4

IMX7ULP-EVK U-boot log:

U-Boot 2018.03-imx_v2018.03_4.14.78_1.0.0_ga+g654088cc21 (Jan 25 2019 - 11:00:58 +0000)

CPU: Freescale i.MX7ULP rev2.0 at 500 MHz
Reset cause: POR
Boot mode: Dual boot
Model: NXP i.MX7ULP EVK
DRAM: 1 GiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
No panel detected: default to HX8363_WVGA
Display: HX8363_WVGA (480x854)
Video: 480x854x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0 is current device
flash target is MMC:0
Net: Net Initialization Skipped
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
** Unable to read file boot.scr **
7248912 bytes read in 358 ms (19.3 MiB/s)
Booting from mmc ...
21429 bytes read in 15 ms (1.4 MiB/s)
263432 bytes read in 27 ms (9.3 MiB/s)
## Booting kernel from Legacy Image at 64000000 ...
Image Name:
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 263368 Bytes = 257.2 KiB
Load Address: 64000000
Entry Point: 64000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 63000000
Booting using the fdt blob at 0x63000000
Loading Kernel Image ... OK
Using Device Tree in place at 63000000, end 630083b4

Starting kernel ...

E/TC:0 dt_overwrite:60 Cannot find fsl,optee-lpm-sram node in the device tree
E/TC:0 dt_overwrite:60 Cannot find fsl,optee-lpm-sram node in the device tree
E/TC:0 plat_rng_init:354 Warning: seeding RNG with zeroes
Booting Linux on physical CPU 0xf00
Linux version 4.14.78-imx_4.14.78_1.0.0_ga+g66620c3d281c (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Fri Jan 25 09:35:37 UTC 2019
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: div instructions available: patching division code
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: NXP i.MX7ULP EVK
Memory policy: Data cache writealloc
Reserved memory: created CMA memory pool at 0x92000000, size 192 MiB
OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
DT missing boot CPU MPIDR[23:0], fall back to default cpu_logical_map
psci: probing for conduit method from DT.
psci: PSCIv0.2 detected in firmware.
psci: Using standard PSCI v0.2 function IDs
psci: MIGRATE_INFO_TYPE not supported.
percpu: Embedded 16 pages/cpu @bf677000 s35532 r8192 d21812 u65536
Built 1 zonelists, mobility grouping on. Total pages: 251650
Kernel command line: console=ttyLP0,115200 root=/dev/mmcblk0p2 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 793580K/1014784K available (9216K kernel code, 505K rwdata, 3200K rodata, 1024K init, 442K bss, 24596K reserved, 196608K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xc0000000 - 0xff800000 (1016 MB)
lowmem : 0x80000000 - 0xbff00000 (1023 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80a00000 (10208 kB)
.init : 0x80e00000 - 0x80f00000 (1024 kB)
.data : 0x80f00000 - 0x80f7e640 ( 506 kB)
.bss : 0x80f80000 - 0x80fee8e0 ( 443 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
Tasks RCU enabled.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
i.MX7ULP clock tree init done.
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: imx-tpm: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 15, mpidr 80000f00
Setting up static identity map for 0x60100000 - 0x60100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
smp: Brought up 1 node, 1 CPU
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
random: get_random_u32 called from bucket_table_alloc+0x114/0x23c with crng_init=0
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 256 (order: 2, 16384 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
mxs_phy 40350000.usbphy: 40350000.usbphy supply phy-3p0 not found, using dummy regulator
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx7ulp-pinctrl 40ac0000.iomuxc1: initialized IMX pinctrl driver
MU is ready for cross core communication!
fsl-edma 40080000.dma-controller: fsl_edma2_irq_init Found 17 interrupts
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: LPI2C adapter registered
i2c i2c-1: LPI2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
MIPI CSI2 driver module loaded
MU is ready for cross core communication!
platform 40000000.ahb-bridge0: coherent DMA mask is unset
virtio_rpmsg_bus virtio0: rpmsg host is online
platform 40000000.ahb-bridge0: coherent DMA mask is unset
virtio_rpmsg_bus virtio1: rpmsg host is online
imx rpmsg driver is registered.
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource imx-tpm
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: no irqs for PMU, sampling events not supported
hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available
Bus freq driver module loaded
workingset: timestamp_bits=30 max_order=18 bucket_order=0
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
pwm-backlight backlight: backlight supply power not found, using dummy regulator
mipi_dsi_northwest 40a90000.mipi_dsi: i.MX MIPI DSI driver probed
adv7535 probing phase
adv7535 0-003d: main addr = 0x3d
i2c i2c-0: ADV7535 not found
mxsfb 40aa0000.lcdif: 40aa0000.lcdif supply lcd not found, using dummy regulator
mipi_dsi_northwest 40a90000.mipi_dsi: MIPI DSI dispdv inited
mxsfb 40aa0000.lcdif: registered mxc display driver mipi_dsi_northwest
Console: switching to colour frame buffer device 80x30
sii902x bound to mxs-lcdif from 40aa0000.lcdif
mxsfb 40aa0000.lcdif: initialized
SW1: failed to get the current voltage(-22)
pf1550-rpmsg pf1550-rpmsg: Failed to initialize regulator-0
pf1550-rpmsg: probe of pf1550-rpmsg failed with error -22
402d0000.serial: ttyLP0 at MMIO 0x402d0010 (irq = 40, base_baud = 1500000) is a FSL_LPUART
console [ttyLP0] enabled
fsl-lpuart 402d0000.serial: NO DMA tx channel, run at cpu mode
fsl-lpuart 402d0000.serial: NO DMA rx channel, run at cpu mode
40a60000.serial: ttyLP2 at MMIO 0x40a60010 (irq = 48, base_baud = 3000000) is a FSL_LPUART
imx sema4 driver is registered.
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
libphy: Fixed MDIO Bus: probed
CAN device driver interface
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 40330200.usbmisc: 40330200.usbmisc supply vbus-wakeup not found, using dummy regulator
input: rpmsg-keys as /devices/platform/rpmsg-keys/input/input0
input: fts_ts as /devices/platform/40800000.ahb-bridge1/40a50000.lpi2c7/i2c-1/1-0038/input/input1
input: step_detector as /devices/platform/rpmsg-sensor/input/input2
input: step_counter as /devices/platform/rpmsg-sensor/input/input3
imx_rpmsg_rtc rtc-rpmsg: rtc core: registered rtc-rpmsg as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 40370000.usdhc: Got CD GPIO
caam 40240000.caam: ERA source: CCBVID.
caam 40240000.caam: device ID = 0x0a16030100000000 (Era 9)
caam 40240000.caam: job rings = 1, qi = 0, dpaa2 = no
RNG Instantation done by Secure Firmware
caam algorithms registered in /proc/crypto
caam_jr 40241000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 8 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] b5 80 4b 0b e3 dc 7c 66
platform caam_sm: [0008] c5 d0 b8 4c 9f 55 5a dd
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] db 80 ec f6 57 51 c3 88
platform caam_sm: [0008] 07 b5 f9 72 b7 b9 4c 8b
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 73 5f 6f 15 29 5a c2 4f
platform caam_sm: [0008] cb ed 0a 01 92 27 93 42
platform caam_sm: [0016] e8 4f da 9a f1 f0 ae f2
platform caam_sm: [0024] 9e 15 24 18 a4 76 89 f2
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] a5 12 35 ed 79 79 df c3
platform caam_sm: [0008] 76 14 d1 a4 8f 99 22 18
platform caam_sm: [0016] cd 90 54 67 35 6d e7 a9
platform caam_sm: [0024] 2d 11 96 ff b9 22 2e 76
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 33 9c 9f d0 60 f3 02 36
platform caam_sm: [0008] fc 4c c7 4b 6d 71 2d c2
platform caam_sm: [0016] 2e ec 91 93 2f 60 d1 2c
platform caam_sm: [0024] 2a 49 bb a8 e7 d7 af c4
platform caam_sm: [0032] 79 d4 32 1a 2b 1c 39 b8
platform caam_sm: [0040] d9 19 c7 e5 ba ac f3 8d
platform caam_sm: [0048] 3f f4 ce da 17 d2 29 14
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] b1 40 49 8e 2d 60 2d 6b
platform caam_sm: [0008] 49 df 72 0a 33 a0 4c 7a
platform caam_sm: [0016] 8a 28 ac 3b 22 ba 0e 82
platform caam_sm: [0024] 64 ce 95 82 d6 bd bb bb
platform caam_sm: [0032] d3 2e e9 2b 54 dd 73 5e
platform caam_sm: [0040] f3 5d 3b b3 54 dd 4b 1d
platform caam_sm: [0048] 8b 96 89 62 d4 d3 35 93
platform caam_sm: [0056] 27 d6 a0 c0 f7 2f d4 f8
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 1c 84 7b a6 a1 7b ef c0
platform caam_sm: [0008] ea 36 56 a8 c0 5a 7f 11
platform caam_sm: [0016] ca 41 96 14 2b 7b dc ff
platform caam_sm: [0024] 14 10 5a d6 02 11 c6 34
platform caam_sm: [0032] 12 bc 29 f9 2b 8b d3 b0
platform caam_sm: [0040] 05 fd 70 29 23 99 a1 25
platform caam_sm: [0048] 0a 8e 46 6f 78 80 20 cf
platform caam_sm: [0056] b3 53 8c c5 58 e4 61 60
platform caam_sm: [0064] aa 43 84 b7 84 64 94 ce
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 65 97 28 a4 5a 7c 81 e8
platform caam_sm: [0008] 03 fa dd 64 9d d8 89 9e
platform caam_sm: [0016] c8 33 e8 70 55 38 8f 94
platform caam_sm: [0024] f7 a9 b6 e7 35 31 4f 8a
platform caam_sm: [0032] 3b 75 1e f5 ad 51 36 e2
platform caam_sm: [0040] c2 d1 e4 54 05 9c dd 2b
platform caam_sm: [0048] dd ac cf a1 af 30 1f dc
platform caam_sm: [0056] 31 ff 17 35 03 50 ce 82
platform caam_sm: [0064] ff 74 7a c4 aa d6 6f f9
platform caam_sm: [0072] 33 c5 3a 5a 40 5c e7 66
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 51 fe 85 d3 0c 86 bd 36
random: fast init done
platform caam_sm: [0008] 75 b5 66 f5 44 14 ae 85
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] db 80 ec f6 57 51 c3 88
platform caam_sm: [0008] 07 b5 f9 72 b7 b9 4c 8b
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 73 5f 6f 15 29 5a c2 4f
platform caam_sm: [0008] cb ed 0a 01 92 27 93 42
platform caam_sm: [0016] 36 9b 1e 3b 69 8a bb 6b
platform caam_sm: [0024] 80 8f 61 77 48 de 98 e4
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] a5 12 35 ed 79 79 df c3
platform caam_sm: [0008] 76 14 d1 a4 8f 99 22 18
platform caam_sm: [0016] cd 90 54 67 35 6d e7 a9
platform caam_sm: [0024] 2d 11 96 ff b9 22 2e 76
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
optee: probing for conduit method from DT.
optee: initialized driver
NET: Registered protocol family 26
NET: Registered protocol family 10
Segment Routing with IPv6
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
Key type dns_resolver registered
cpu cpu0: failed to get regulator
imx7ulp-cpufreq: probe of imx7ulp-cpufreq failed with error -2
gpio-reset modem-reset: failed to request gpio 143: -22
gpio-reset: probe of modem-reset failed with error -22
WLAN_EN: Failed to request enable GPIO142: -22
reg-fixed-voltage regulators:sd1_regulator: Failed to register regulator: -22
reg-fixed-voltage: probe of regulators:sd1_regulator failed with error -22
sdhci-esdhc-imx 40370000.usdhc: Got CD GPIO
imx_rpmsg_rtc rtc-rpmsg: hctosys: unable to read the hardware clock
usb_otg1_vbus: disabling
VSD_3V3: disabling
ALSA device list:
No soundcards found.
Waiting for root device /dev/mmcblk0p2...

标签 (1)
3 回复数

2,174 次查看
vanessa_maegima
NXP Employee
NXP Employee

Hi chum,

Did you flash the .sdcard image to your sd card using dd commands?

dd if=<your_image>.sdcard of=/dev/sdX

sdX refers to your sd card.

It seems that kernel cannot find your rootfs partition. After flashing, it should be in the ext4 partition.


Vanessa

2,174 次查看
chum
Contributor III

Hi Vanessa,

I found problem, when i do dd if=<your_image>.sdcard of=/dev/sdX all files copied to sd card properly and when i load the yocto build demo M4 .img file both the cores working properly. to load i use this command

=> sf probe

=> sf erase 0x0 0x20000

=> fatload mmc 0:1 0x62000000 imx7ulp_m4_demo.img

=> sf write 0x62000000 0x0 0x20000

its working properly and A7 loads with linux, M4 with power_mode_switch application. 

A7_M4.PNG

------------------

Error case:

I'm following this link to build freeRtos image -How to build and flash a bootable image for Cortex-M4 on i.MX 7ULP - i.MXDev Blog 

To build .img i run - ./mkimg.sh flash

=> sf probe

=> sf erase 0x0 0x20000

=> fatload mmc 0:1 0x62000000 sdk20-app.img

=> sf write 0x62000000 0x0 0x20000

A7 problem occur like below:(M4 working as expected)

A7_M4_error.PNG

SDcard image used : core-image-base-imx7ulpevk-20190129083130.rootfs.sdcard

uboot from RAW partition, linux image from FAT partition, root file system from ext4 partition

0 项奖励
回复

2,174 次查看
vanessa_maegima
NXP Employee
NXP Employee

Hi chum,

This occurs as the M4 image you loaded (Hello World) does not provide all needed configuration to boot with A7.

The SDK demo that provided the needed power initialization to boot A7 along with M4 is the power_mode_switch (the same as provided by Yocto build).

Another option is to boot the board in Single Boot mode. In this mode, A7 kicks M4 and does not expect the initialization from M4 anymore and you can run the Hello World demo along with A7 + Linux. For Single Boot mode procedure, please see i.MX 7ULP Heterogeneous Architecture and Different Boot Modes - i.MXDev Blog .

Best,

Vanessa

0 项奖励
回复