IMX7SOLO - NVCC_SD1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7SOLO - NVCC_SD1

1,132件の閲覧回数
testaluca82
Contributor I

In the datasheet (IMX7SCEC) on Table 87 the power supply for SD1 is not mentioned.

We can find it on Table 89 at J11.

I would just like to point it out in case someone is looking for it !

Maybe NXP will update the documantation later on...

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,065件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Thank for the information. The line with NVCC_SD1 (J11) is included for
table "i.MX 7Solo 12 x 12 mm supplies contact assignments"  modification

by the doc team.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信