IMX7DSABRESD JTAG INTERFACE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7DSABRESD JTAG INTERFACE

2,285 Views
raviranjankumar
Contributor III

Hi all,

I am working on IMX7 Dual SABRE board. I want to debug Cortex-M4 core through JTAG in IAR workbench. I tried with I-JET and PE-Micro debugger but I am not able to flash. 

What are the steps I need to follow if I want to debug it through JTAG? 

Any settings or configuration I need to do on the board or in IAR.

Please help...

Thanks and Regards,

Ravi Ranjan Kumar.

0 Kudos
Reply
3 Replies

2,093 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ravi

one can look at

Debugging Cortex-M4 on i.MX7D with Segger J-Link and GDB (and thus standard Eclipse) 

https://www.embeddedartists.com/sites/default/files/support/com/iMX7_Working_with_Cortex-M4.pdf 

AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK

https://www.nxp.com/docs/en/application-note/AN5229.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,093 Views
raviranjankumar
Contributor III

Hi, igorpadykov,  

Thanks for your valuable information. I have gone through those documents, there is not enough information for IAR. In some documents, it is given that create a bin file and upload (It is working fine).  But can I debug it directly in Keil or IAR using PE-Micro or I-Jet?

I am using VCC, TMS, TCK, nRES, GND pin in JTAG, is it correct?

Please guide...

Thanks and regard,

Ravi Ranjan Kumar.

0 Kudos
Reply

2,093 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ravi

for using these debug tools suggest to contact its vendor tech support:

PE-Micro

PEmicro | Experts in Embedded tools for Flash Programming and Development 

Keil

Keil Product Support 

Best regards
igor

0 Kudos
Reply