IMX7D to LPDDR3 interface clock termination

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7D to LPDDR3 interface clock termination

1,410件の閲覧回数
logeshs
Contributor II

Hi,

We are using MCIMX7D3EVK10SD in our design with 08EMCP08-EL3DT227-A01U (Kingston Memory) using LPDDR3 interface. 

Kindly suggest what type termination need to be provided for DDR_Clock in  LPDDR3 interface. I could not find any recommendation for DDR_Clock Termination and in WARP board design no termination was used. Kindly suggest suitable termination or shall we connect as such in WARP schematics design.

Thanks & Regards,

Logesh

ラベル(1)
0 件の賞賛
返信
1 返信

1,235件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Logesh

please refer to sect.3. i.MX7 series layout recommendations Hardware Development

Guide for i.MX7Dual and 7Solo Applications Processors, termination is not used.
http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf

In general recommended to perform signal integrity (SI) simulations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信