IMX7D GPIO on manul reset input of the reset IC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX7D GPIO on manul reset input of the reset IC

1,415 次查看
frankyhsu
Contributor III

We use GPIO1_IO0 and IO1 as the reset MR input, we know the IO0 is internal pull up but IO1 is internal pull down. Do we have method to let IO1 to be pulled high? It seems there is only IO0 that has internal pulled up. The internal pull down will let reset IC continue to reset.

标签 (1)
0 项奖励
回复
3 回复数

1,223 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Franky

 

out of reset state is described on Table 100. i.MX 7Dual 19 x 19 mm functional

contact assignments i.MX7D Datasheet

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf

and there is no way to change that behaviour immediately after power-up.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,223 次查看
frankyhsu
Contributor III

Could we use pull high on this pin to change the initial status?

0 项奖励
回复

1,224 次查看
igorpadykov
NXP Employee
NXP Employee

in general yes, it can be overriden with external pull resistor.

~igor

0 项奖励
回复