IMX7D ESPI slave mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D ESPI slave mode

6,510 Views
chandiniindavar
Contributor IV

Hi

I am planning to connect 2 IMX7D boards through SPI.

I refereed below link. which is for imx6 espi as salve with 3.0.35_4.1.0 kernel

i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0

But i am using new 4.1.15 kernel . i tried to search similar files for imx7d . but couldn't find it.

when i configure slave master i just changed imx7d-sdb.dts and got it running .

Could any one please tell me what to do with newer kernel ?

Thank you

Chandini

Labels (5)
0 Kudos
Reply
7 Replies

5,160 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chandini

please try patch on

[PATCH v2 8/8] spi: imx: Add support for SPI Slave mode for imx53 and imx6 chips | Linux | Kernel

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,161 Views
deven_solanki
Contributor III

Hi Igor,

Could you please share SPI-SLAVE patch for Linux_4.9.11?

Best regards

Solanki Deven

0 Kudos
Reply

5,161 Views
gonewithwind-peter
Senior Contributor I

did you make it work well. can you share your work? thank you. I did like my upper post. do not work well.

0 Kudos
Reply

5,161 Views
chris_f
Contributor V

igorpadykov‌ I'm trying to get SPI slave working on 4.1.15. Lots of the patch that you suggested can be applied but plenty of it can't.

Do you know if anyone has updated this?

0 Kudos
Reply

5,161 Views
igorpadykov
NXP Employee
NXP Employee

please check i.MX7 eCSPI driver discussion on

spi drivers for Colibri imx7 dual - Toradex Community 

Best regards
igor

5,159 Views
chandiniindavar
Contributor IV

Hi Igor

I apply patch successfully by solving few compilation errors.and build zimage

but i have few questions.

1. Do i need to change anything in imx7d-sdb.dts ?

2. Do i need to add any configuration ?

     currently i am enabling just below 2 options :

     Device Drivers > SPI Support > Utilities for Bitbanging SPI masters.

     Device Drivers > SPI Support > Freescale i.MX SPI controllers.

3. once i got spi slave working.  how device looks like in board? i mean ,is it something similar master SPI[ ex: spidev2.0 ] ?

i copied zimage to sdcard but i could not see any device . i have attached my 2 files what i have changed.

I got below link which talk about 8 patchs for spi-slave support . it includes link the one which you suggested me . is it helpful ?

Linux-Kernel Archive: [PATCH v2 0/8] Improvements for SPI IMX driver for Freescale IMX53 and IMX6 fa...

Thank you

Chandini

0 Kudos
Reply

5,159 Views
gonewithwind-peter
Senior Contributor I

hi 

I used your patch for board imx7: https://www.arrow.com/en/products/pico-pi-imx7-amazon/technexion   which is ecspi3. it can pass the compilation

and I modified the device tree as following in file imx7s.dtsi:

...
ecspi3: ecspi@30840000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx7d-ecspi", "fsl,imx51-ecspi";
reg = <0x30840000 0x10000>;
interrupts = <GIC_SPI 33 IRQ_TYPE_LEVEL_HIGH>;
fsl,spi-num-chipselects = <1>;
fsl,spi-slave-mode;
clocks = <&clks IMX7D_ECSPI3_ROOT_CLK>,
<&clks IMX7D_ECSPI3_ROOT_CLK>;
clock-names = "ipg", "per";
dmas = <&sdma 4 4 0>, <&sdma 5 4 0>;
dma-names = "rx", "tx";
status = "okay";
spidev@0 {
compatible = "spidev";
reg = <0>;
spi-max-frequency = <20000000>;
};
};

...

but the spi slave can not works well. I used the  spidev-test/spidev_test.c at master · rm-hull/spidev-test · GitHub    to test it.

I 

cat /proc/interrupts | grep spi

52:          1          0     GPCV2  33 Edge      30840000.ecspi

only 1 interrupt happened. I think if input continuously, It should be many interrupts happened.

Did you make it work well?

what i missed?

thank you for your reply to : [email protected]

0 Kudos
Reply