IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7

3,829 Views
jovi
Contributor I

where find default configuration IMX7

0 Kudos
Reply
8 Replies

3,494 Views
jovi
Contributor I

Small curiosite:
Is it possible to download an already built Debian ISO image and simply copy and install it on the NXP IMX7 Dual Sabre processors SD card? as with a raspberry pi

0 Kudos
Reply

3,494 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, you can download the imx7 demo images, which includes these pre-built demo image, you also can find them in the mfgtool

0 Kudos
Reply

3,494 Views
jovi
Contributor I

def_config image1.PNG

In section c: Download and make the kernel and dtb
after downloading and unzipping the kernel link
I made the command make imx_v7_defconfig
but I received the errors described on the picture above.

Thanks

0 Kudos
Reply

3,494 Views
jovi
Contributor I

thank you very much, but I was already following the Kane Jiang tutorial in the NXP community to install Debian 8 Jessie Rootfs on the NXP i.MX6ULL EVK board, but the only difference is that I would like to do it on the IMX 7Dual Saber board, I do It  well in the beginning, but up to section c: Download and make the kernel and dtb, I receive compilation errors and I am a little lost.

Here is the link to the tutorial: https://community.nxp.com/docs/DOC-334274.

Thanks

0 Kudos
Reply

3,494 Views
joanxie
NXP TechSupport
NXP TechSupport

what error do you get? pls share with me

0 Kudos
Reply

3,494 Views
jovi
Contributor I

I mean the software configuration,
in fact i would like to download and make debian linux kernel, a dtb file for the IMX7 Sabre sd of NXP.

And I block at the default software configuration of the Board

Thanks

0 Kudos
Reply

3,496 Views
joanxie
NXP TechSupport
NXP TechSupport

for how to find the sw configuration you can refer to the linux refence manual for detailed module,. for yocto, you can refer to the traning as below, tell you how to find the menu configuration

https://community.nxp.com/docs/DOC-95045 

0 Kudos
Reply

3,496 Views
joanxie
NXP TechSupport
NXP TechSupport

what  configuration do you mean? for HW or SW?

0 Kudos
Reply