IMX7 linux kernel freezing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7 linux kernel freezing?

2,700件の閲覧回数
jjamesson
Contributor II

Hi, Community,

I am having an issue running Linux kernel on a custom hardware board, and I'm reaching out to get help. It seems that Linux is starting correctly, but then ends up freezing/stalling at some point, as I am not able to do anything beyond this point, including writing to terminal. This same build, however, works on the IMX7 Sabre board using only a different DDR config.

I have debugged it so far that I know that the stalling happens in cpu_startup_entry() function in linux-imx/init/main.c. Furthermore, I have attached the minicom output, where the stalling happens after the very last command.

Is this definitely a DDR configuration related issue?

With regards,

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,637件の閲覧回数
jjamesson
Contributor II

Issue resolved!
I fixed it by removing any irrelevant peripherals in the device tree for Linux.

Thank you, and this issue can be closed.

0 件の賞賛
返信

2,637件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello James Jamesson,

Thank you for updating this thread and letting us know what the problem was! Hopefully it may help other community users.

Regards,

0 件の賞賛
返信

2,637件の閲覧回数
jjamesson
Contributor II

Status update:

I checked the DDR configuration with the stress tester tool, and it passed the test. So this problem is unlikely a DDR configuration problem.

0 件の賞賛
返信