IMX7 M4 cache

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7 M4 cache

2,543件の閲覧回数
dry
Senior Contributor I

Hey YuriMuhin_ng

Yuri Muhin wrote:

 

  The CACHE for the CM4 is not functioning on the rev 1.0 silicon.

 Also, please refer to RTOS sources how to work with LMEM.

Was this fixed for rev  >= 1.2 ? 

Thanks in advance 

0 件の賞賛
返信
2 返答(返信)

2,196件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, the CM7 cache is working.

From the team:

The cache is working in later revisions. Also, there are no CM4 cache specific issues in the errata.

 

Some issues that are on the community that are related to the CM4 cache:

 

Unable to use breakpoints on iMX7D when firmware placed in OCRAM...  , but this one has a workaround.

 

Re: i.MX7D: atomic compare and swap instructions don't work with cache , but this issue is not be treated

as a silicon bug and the document https://community.nxp.com/docs/DOC-340245 

describes how to work around it.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信

2,196件の閲覧回数
dogisfat
Contributor IV

Yuri,

The document Arm Cortex-M4™ Exclusive Access Support for i.MX Processors doesn't seem to exist or is inaccessible. Could you fix the link?

0 件の賞賛
返信