IMX7 Hypervisor mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,907件の閲覧回数
shammi112
Contributor I


Hi,

I want to make use of KVM feature of linux kernel. Is there any document or patch to boot imx7 into hypervisor mode.

0 件の賞賛
返信
1 解決策
5,552件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

according to the following Processor support - KVM :

"Virtualization support for ARM was initially added to ARMv7-A
processors starting with Cortex-A15 and including Cortex-A7 ..."

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
5,552件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NXP does not support hypervisor technology for i.MX series, but

customers can try using KVM feature of Linux kernel.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,552件の閲覧回数
shammi112
Contributor I

Hi,

I want to know whether Imx7 boots in secure or non-secure world once it comes out of reset.

0 件の賞賛
返信
5,552件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"After power on reset (POR), in Secure World, all interrupts are secure interrupts, all

bus masters are configured as Secure World masters, and all bus slaves can be

accessed by Secure World bus masters. [...]. If a trusted execution environment is not
required, there is no need to switch to Normal World."

Regards,

Yuri.

0 件の賞賛
返信
5,552件の閲覧回数
shammi112
Contributor I

Hello,

OK Thanks, so we need to boot CPU in non-secure state for Hypervisor mode.

Regards,

SHAMMI

0 件の賞賛
返信
5,552件の閲覧回数
shammi112
Contributor I

Hi,

But to make best use of KVM CPU should boot in hypervisor mode. cortex a7 does support hypervisor mode. Is there any reference document which will boot cortex a7 CPU in hypervisor mode.

0 件の賞賛
返信
5,553件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

according to the following Processor support - KVM :

"Virtualization support for ARM was initially added to ARMv7-A
processors starting with Cortex-A15 and including Cortex-A7 ..."

Regards,

Yuri.

0 件の賞賛
返信