mfg-tool stuck on Sending partition shell

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfg-tool stuck on Sending partition shell

1,788件の閲覧回数
adriaanswanepoe
Contributor I


We are using the mfg-tool to setup a custom board based on the iMX6Q.

We have built updated versions of the mfg U-Boot, kernel, root file system, and device tree for our HW.

The mfg-tool detects the board when powered up, sends U-Boot, kernel, rfs and dtb and successfully jumps to U-Boot.

U-Boot successfully starts the kernel and the mass storage device comes up.

When the mfg-tool tries to execute the push send for mksdcard_new.sh.tar (Sending partition shell) step but gets stuck with no debug on the device.

Any recommendations, ideas, debug I need to provide?

Thanks,

Adriaan

ラベル(2)
0 件の賞賛
返信
1 返信

1,549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Adriaan

if baord stucks with no debug this may be due to memory errors.

https://community.freescale.com/docs/DOC-105652

Also one can try to execute these commands from linux, as mfg tools just runs

small linux image.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信