IMX7 ECSPI transfer error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 ECSPI transfer error

Jump to solution
2,623 Views
asmaa
Contributor V

Hello Everyone,

I am working on imx7d, the kernel is 4.19.35-00034-g261c3547e33e-dirty.

I have written a slave driver, which can successfully send and receive 16 bytes of data. However, when I am trying to read data of 34 bytes. I am getting the following error.

imx-sdma 30bd0000.sdma: sdma firmware not ready!
maxq1744 spi3.0: SPI transfer failed: -22
spi_master spi3: failed to transfer one message from queue
Error while sending data = -22

When I initially did grep search on sdma I found this

root@qt850:~# dmesg | grep sdma
[ 0.383866] imx-sdma 30bd0000.sdma: no iram assigned, using external mem
[ 0.384229] imx-sdma 30bd0000.sdma: Falling back to syfs fallback for: imx/sdma/sdma-imx7d.bin
[ 6.024038] imx-sdma 30bd0000.sdma: external firmware not found, using ROM firmware

My device tree is as follows:

&ecspi4 {
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi4 &pinctrl_ecspi4_cs>;
cs-gpios = <&gpio5 3 GPIO_ACTIVE_LOW>;
status = "okay";

spidev1: spi@0 {
compatible = "quest,maxq1744";
reg = <0>;
spi-max-frequency = <100000>; /* MAXQ1744, When configured for SPI operation operates as an SPI slave,
supporting an SPI clock of up to 250 kHz*/
msr-supply = <&msr_power>;
rst-gpios = <&gpio6 14 GPIO_ACTIVE_HIGH>; /*An external reset is activated when the pin is held low for more than 400 μs.*/
interrupt-parent = <&gpio5>;
interrupts = <7 IRQ_TYPE_EDGE_FALLING>;
};
};

I get the interrupt correctly, I am just having issues when I am trying to read data greater than 16 bytes.

My question is as follows:

I am not using any dmas in my slave driver. Is it ok for transfer more than 16 bytes not to use dma?

What could possibly the reason for this error?

maxq1744 spi3.0: SPI transfer failed: -22
spi_master spi3: failed to transfer one message from queue

Looking forward to your response?

Regards,

Asma

Labels (1)
0 Kudos
Reply
1 Solution
2,571 Views
igorpadykov
NXP Employee
NXP Employee

Hi Asma

as workaround one can try to remove dma entries in dts file:

imx7s.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,572 Views
igorpadykov
NXP Employee
NXP Employee

Hi Asma

as workaround one can try to remove dma entries in dts file:

imx7s.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply