IMX6solo -Unable to Boot EMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6solo -Unable to Boot EMMC

1,384 次查看
ericyeoh
Contributor I

I am using an imx6solo and an emmc at usdhc4, below are my initialise script, somehow the i cannot detect the emmc that attached in the system.

anyone  can help?

mem write 0x20E0338 0x0 ;IOMUXC_SW_MUX_CTL_PAD_SD4_CLK  ;select sd4_clk,

mem write 0x20E0720 0x17059

mem write 0x20E033C 0x10; IOMUXC_SW_MUX_CTL_PAD_SD4_CMD; select sd4_cmd,             

mem write 0x20E0724 0x17059           

mem write 0x20E0340 0x1 ;IOMUXC_SW_MUX_CTL_PAD_SD4_DATA0; select  sd4_data0,          

mem write 0x20E0728 0x17059

mem write 0x20E0344 0x1 ;IOMUXC_SW_MUX_CTL_PAD_SD4_DATA1; select sd4_data1,                  

mem write 0x20E072C 0x17059               

mem write 0x20E0348 0x1 ;IOMUXC_SW_MUX_CTL_PAD_SD4_DATA2; select sd4_data2,                

mem write 0x20E0730 0x17059             

mem write 0x20E034C 0x1 ;IOMUXC_SW_MUX_CTL_PAD_SD4_DATA3; select sd4_data3,              

mem write 0x20E0734 0x17059 

mem write 0x20E0350 0x1     ;sd4

mem write 0x20E0738 0x17059

mem write 0x20E035C 0x01    ; sd7

mem write 0x20E0744 0x17059

mem write 0x20E0354 0x01    ;sd5

mem write 0x20E073C 0x17059

mem write 0x20E0358 0x01    ;sd6

mem write 0x20E0740 0x17059

mem write 0x20E0278 0x01    ;NANDF_CS1, sd4_vselect

mem write 0x20E0660 0x171C1

mem write 0x20E026C 0x01    ;NANDF_ALE , sd4 reset

mem write 0x20E0654 0x171C1

0 项奖励
回复
1 回复

1,181 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

first please verify that sion bid is set for emmc iomux settings, then

please use Manufacturing Tool for programming emmc:

Programmers (Flash, etc.) (9)

IMX6_L3.14.52_MFG_TOOL (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复