IMX6sd + linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6sd + linux

1,524件の閲覧回数
nlsainath
Contributor I

Hi,

I have compiled the dts supported uboot which is compiled to imx6q sabre sd board. Also compiled the kernel 3.10 where I have the dts & uImage. Now I want to make a bootable SD card. Can anyone give me script to create partitions & load the images.

uboot environment parameters that needs to be set..

Regards

Sainath.

0 件の賞賛
返信
1 返信

1,409件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sainath

you can find scripts included in IMX_6_MFG_L3.10.17_1.0.0_TOOL

uboot environment parameters and procedure for creating sd image

can be found in i.MX_6_SABRE-SD_Linux_User's_Guide.pdf,

i.MX_6_SABRE-SD_Linux_Release_Notes.pdf included in

L3.10.17_1.0.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信