IMX6ULL with codec MAX98090

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL with codec MAX98090

3,215 Views
dc1
Contributor II

Hello all,

i need to configure the IMX pin that control the LRCLK pin of the MAX98090 as outpout beacuse i have problem with the clock signal levels. For the MCLK we have do that in this way:

pastedImage_1.png

how can i do the same for the LRCLK pin that is connected to the SAI_SYNC pin?

Thanks

0 Kudos
Reply
4 Replies

3,107 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniele

one can look at i.MX6ULL EVK wm8960 example :

imx6ull-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

i.MX6ULL EVK schematic

Design files, including hardware schematics, Gerbers, and OrCAD files

may be useful to check sai dts documentation:

fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,107 Views
dc1
Contributor II

Hello,

thanks we are trying to understand if the configuration of the pins is correct for our MAX98090 that is different from the wm8960 . We have set the fsl,pins in this way:

 pinctrl_sai2: sai2grp {
                        fsl,pins = <
                                MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK        0x170A1
                                MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC        0x170A1
                                MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA     0x110A0
                                MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA        0x110A0
                                MX6UL_PAD_JTAG_TMS__SAI2_MCLK           0x170A1
                        >;
                };

 reducing the DSE resistence and enabling the fast slew rate 

pastedImage_1.png

we have seen that the PAD define are:

/*
 * The pin function ID is a tuple of
 *                                                                                                 <mux_reg conf_reg input_reg mux_mode input_val>
 */
#define MX6UL_PAD_SD1_CLK__SAI2_MCLK                          0x01C0   0x044C   0x05F0   0x2         0x1
#define MX6UL_PAD_SD1_DATA0__SAI2_TX_SYNC               0x01C4   0x0450   0x05FC   0x2         0x1
#define MX6UL_PAD_SD1_DATA1__SAI2_TX_BCLK               0x01C8    0x0454   0x05F8   0x2         0x1  
#define MX6UL_PAD_SD1_DATA2__SAI2_RX_DATA                0x01CC   0x0458   0x05F4   0x2         0x1
#define MX6UL_PAD_SD1_DATA3__SAI2_TX_DATA                0x01D0   0x045C   0x0000   0x2          0x0
with the value written in the fsl,pins (for example the 0x170A1) we are going to over-write a value of the #define here upper or what?
Thanks
0 Kudos
Reply

3,107 Views
igorpadykov
NXP Employee
NXP Employee

so had you checked signals with oscilloscope,

do they suit MAX98090 datasheet requirements ?

Best regards
igor

0 Kudos
Reply

3,107 Views
dc1
Contributor II

Hello,

we are trying to increase the clock signal quality changing the DSE configuration of the pins following the guide on pag 19 of this document https://docs.toradex.com/104446-colibri-arm-som-imx6ull-datasheet.pdf 

Thanks

0 Kudos
Reply