IMX6ULL uboot Error: Invalid IVT structure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL uboot Error: Invalid IVT structure

2,080件の閲覧回数
rohitkumar21
Contributor I

Hi There,

I'm trying to enable High Assurance Boot on my device. I'm using buildroot and initially I only enabled the CONFIG_SECURE_BOOT=y in uboot_menuconfig. Now I'm getting error in uboot, "Error: Invalid IVT structure". I'm not using a signed image for now, once I get the uboot booting right I'll flash signed image.

I tried to extract the IVT structure using genIVT.pl script. With that I'm getting following output:


Kernel = /home/IMX/hab/ivt_test-2/zImage
IVT = /home/IMX/hab/ivt_test-2/ivt.bin
Padded File Size = 0x738000
Kernel file size = 0x737620
Jump location    = 0x80800000
Self Pointer     = 0x80F38000
CSF Pointer      = 0x80F38020

$ hexdump -C ivt.bin
00000000 d1 00 20 41 00 00 80 80 00 00 00 00 00 00 00 00 |.. A............|
00000010 00 00 00 00 00 80 f3 80 20 80 f3 80 00 00 00 00 |........ .......|
00000020


I also tried to print the IVT sturcture values during uboot startup, I'm getting following logs:

U-Boot 2018.03 (Jul 06 2023 - 16:01:57 +0530)

CPU: Freescale i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 53C
Reset cause: POR
Board: devBoard-v1
I2C: ready
DRAM: 512 MiB
LCD model: 1 - AVDTTXXXXXXXXXX
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

auto-detected panel AVDTTXXXXXXXXXX
Display: AVDTTXXXXXXXXX (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
eMMC: 3.6 GiB
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1(part 0) is current device
Loading bootpath.txt from 1:1/bootpath.txt
27 bytes read in 33 ms (0 Bytes/s)
Loaded boot path from bootpath.txt
Importing boot path from mmc ...
Importing bootpath.txt
bootdir=a
mmcrootpart=3
1185 bytes read in 45 ms (25.4 KiB/s)
Importing bootenv from mmc ...
84 bytes read in 59 ms (1000 Bytes/s)
Running bootscript from mmc ...
## Executing script at 82000000
gpio: pin 6 (gpio 6) value is 0
gpio: pin 32 (gpio 32) value is 1
gpio: pin 115 (gpio 115) value is 1
7566880 bytes read in 234 ms (30.8 MiB/s)
Booting from mmc ...
70545 bytes read in 56 ms (1.2 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
hab fuse not enabled

Authenticate image from DDR location 0x80800000...
~~~~~ IVT Sturcture ~~~~~
~~~~~~~~~~~~~~~~~~~~~~~~~
ivt_hdr->magic = 0x61
ivt_hdr->length = 0xA010
ivt_hdr->version = 0xE3

ivt_hdr = 0x80F38000
ivt_entry = 0xC59B21A8
ivt_rsv1 = 0x8020000B
ivt_dcd = 0xC08E3003
ivt_boot = 0xC08F0002
ivt_self = 0xE08C3014
ivt_csf = 0xE0A03008
ivt_rsv2 = 0x58C4018
~~~~~~~~~~~~~~~~~~~~~~~~~
bad magic magic=0x61 length=0xa010 version=0xe3
bad length magic=0x61 length=0xa010 version=0xe3
bad version magic=0x61 length=0xa010 version=0xe3
FAIL: ivt_hdr : 0x80F38000 : verified ivt_header
PASS: ivt_initial->entry : 0xC59B21A8 != 0x0
FAIL: ivt_initial->reserved1 : 0x8020000B != 0x0
FAIL: ivt_initial->self : 0x8020000B != 0x80F38000
PASS: ivt_initial->csf : 0xE0A03008 != 0x0
FAIL: ivt_initial->reserved2 : 0x58C4018 != 0x0
FAIL: ivt_initial->dcd : 0xC08E3003 != 0x0
bad magic magic=0x61 length=0xa010 version=0xe3
bad length magic=0x61 length=0xa010 version=0xe3
bad version magic=0x61 length=0xa010 version=0xe3
Error: Invalid IVT structure

Allowed IVT structure:
IVT HDR = 0x4X2000D1
IVT ENTRY = 0xXXXXXXXX
IVT RSV1 = 0x0
IVT DCD = 0x0
IVT BOOT_DATA = 0xXXXXXXXX
IVT SELF = 0xXXXXXXXX
IVT CSF = 0xXXXXXXXX
IVT RSV2 = 0x0
Using Device Tree in place at 83000000, end 83014390

Starting kernel ...

 

I'm stuck with this invalid IVT structure issue. Kindly let me know where I'm getting things incorrect.

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

2,022件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @rohitkumar21,

I hope you are doing well.

Thanks for the logs, I checked it.
It shows that the IVT structure in the kernel image is invalid. It contains the kernel's secure boot state, so this requirement needs to be validated properly.
If the requirements are not met then U-boot may fail to boot the kernel.

->Please cross-check the magic value, length, version, self, DCD fields, and CSF is correct or not.
After cross-checking it please flash the image again.

I hope it helps!

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信