IMX6ULL Processor canfd clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL Processor canfd clock

1,494 Views
pooja_todakar
Contributor I

hii,

i am installing the tcan4x5x canfd driver processor used is imx6ull,

i had apply cclk(can clock) of 40Mhz.in hardware it is external crystal oscillator,

how can i enable the clock in software?

one host clock given by spi interface.another clock for canfd i have to give.

Labels (1)
0 Kudos
Reply
1 Reply

1,422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pooja

one can look at tcan4x5x schematic and dts example

http://www.ti.com/lit/ug/sllu281a/sllu281a.pdf 

linux/tcan4x5x.txt at master · torvalds/linux · GitHub 

so except spi no other clocks are needed from i.mx side.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply