IMX6ULL NAND flash boot failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL NAND flash boot failed

1,667 Views
allonli
Contributor II

trying to burn image to NAND FLash on IMX6ULL platform by mfgtools_4.1.15,

now stuck on "No device connect".

log info show as below on the left, halted at "configfs-gadget gadget: high-speed config #1: c", 

I try the same operations on IMX6ULL EVK demo board, while the log info show on the right. (IMX6ULL EVK no NAND flash on board)

it seems the utp device have been found, but UTP cammand can not receive or can not excute?

I set USB OTG1 ID floating, and also let dr_mode=peripheral

what could be the reason?

iot gateway

0 Kudos
Reply
1 Reply

1,585 Views
igorpadykov
NXP Employee
NXP Employee

Hi Allon

reason may be that usb is not working on custom board

one can test usb (both host and device mode) using imx-test package,

folder mxc_usb_test

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply