IMX6ULL GPIO function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL GPIO function

Jump to solution
2,194 Views
Saenghee
Contributor I

dear nxp

 

GPIO01_IO01 will connect BT_HOST_WAKE_INT

BT_HOST_WAKE pin will  wake up the AP(IMX6ULL) even if the AP sleep state.

Q1>  GPIO01_IO01 have interrupt function?

        GPIO01_IO01 support AP wakeup?

Q2> ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

        ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

        ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

        ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

0 Kudos
Reply
1 Solution
2,178 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

A1 > Yes, it does

A2 >

ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

Yes, ALT1 mux port: UART8_RTS_B

ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

Yes, ALT1 mux port: UART8_CTS_B

ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

Yes, ALT1 mux port: UART8_TX

ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

Yes, ALT1 mux port: UART8_RX

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
2 Replies
2,175 Views
Saenghee
Contributor I

thank you for your confirmation.

close.

0 Kudos
Reply
2,179 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

A1 > Yes, it does

A2 >

ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

Yes, ALT1 mux port: UART8_RTS_B

ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

Yes, ALT1 mux port: UART8_CTS_B

ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

Yes, ALT1 mux port: UART8_TX

ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

Yes, ALT1 mux port: UART8_RX

Best regards,
Aldo.

0 Kudos
Reply