IMX6ULL GPIO function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL GPIO function

ソリューションへジャンプ
2,201件の閲覧回数
Saenghee
Contributor I

dear nxp

 

GPIO01_IO01 will connect BT_HOST_WAKE_INT

BT_HOST_WAKE pin will  wake up the AP(IMX6ULL) even if the AP sleep state.

Q1>  GPIO01_IO01 have interrupt function?

        GPIO01_IO01 support AP wakeup?

Q2> ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

        ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

        ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

        ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

0 件の賞賛
返信
1 解決策
2,185件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

A1 > Yes, it does

A2 >

ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

Yes, ALT1 mux port: UART8_RTS_B

ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

Yes, ALT1 mux port: UART8_CTS_B

ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

Yes, ALT1 mux port: UART8_TX

ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

Yes, ALT1 mux port: UART8_RX

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,182件の閲覧回数
Saenghee
Contributor I

thank you for your confirmation.

close.

0 件の賞賛
返信
2,186件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

A1 > Yes, it does

A2 >

ENET2_RX_ER support UART RTS function ? (it will connect BT UART CTS)

Yes, ALT1 mux port: UART8_RTS_B

ENET2_TX_CLK support UART CTS function?(it will connect BT UART RTS)

Yes, ALT1 mux port: UART8_CTS_B

ENET2_TX_DATA1 support UART TXD function?(it will connect BT UART RXD)

Yes, ALT1 mux port: UART8_TX

ENET2_TX_EN support UART RXD function? (it will connect BT UART TXD)

Yes, ALT1 mux port: UART8_RX

Best regards,
Aldo.

0 件の賞賛
返信