IMX6ULL ECSPI slave mode data transfer issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL ECSPI slave mode data transfer issue

1,513 Views
liqi_wu
Contributor III

Current i use IXM6ULL SPI as slave mode. But I find the front of 8 bytes in SPI slave send is incorrect.

In this case, bps = 20M, BURST_LENGTH = 32, POL =0, PHA = 0, and SS_CTL[x] = 0. attach SPI configuration.

pastedImage_1.png

//issue description

1. I put below data to SPI TX FIFO:

00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

2. but the front 8 bytes is incorrect.

sometimes as:

00 00 00 00 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

sometimes as:

3C 3D 3E 3F 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

Labels (2)
0 Kudos
Reply
3 Replies

1,377 Views
liqi_wu
Contributor III

This issue is fixed. This question can close now.

The root cause is the SPI burst length are not equal with master and slave.

when I configurate the master SPI and slave SPI burst length is 32bit or 128bit, this issue is disappeared. 

0 Kudos
Reply

1,377 Views
igorpadykov
NXP Employee
NXP Employee

Hi liqi

one can recheck if correct escpi initialization performed in the case,

described in sect.20.5 Initialization i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,377 Views
liqi_wu
Contributor III

Hi igor,

 

Sorry for reply so late.

I use function(ECSPI_SlaveInit) which in SDK_2.2_MCIM6ULL to initiate the ECSPI.

 

The interesting thing is: why the front of four bytes data in SPI slave send is the end four bytes which the data in SPI slave last send?

 

//issue description

  1. I put below data to SPI TX FIFO:

00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

  1. but the front 4 bytes is incorrect.

First sometimes as:

00 00 00 00 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

 

After that sometimes as:

3C 3D 3E 3F 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

sometimes as:

3C 3D 3E 3F 00 00 00 00 08 09 0A 0B 0C 0D 0E 0F 10 11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20 21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30 31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F

 

 

I wonder if it is caused by incorrect configuration or if it is the issue of IMX6ULL?

 

Thanks!

wuliqi

0 Kudos
Reply