IMX6ULL DRR CALIBRATION FAILED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL DRR CALIBRATION FAILED

1,439 Views
Oman
Contributor II

I used ddr_stress_tester to test my pacba, but failed at calibration.

Then,I Set Voltage to 1.75, it tests success.

 

Q1: How do I set voltage to source code?Because  when brushing machine is also failed .so it can not go to the linux system. should I modify DCD data of code on uboot? 

Q2: for his failed of calibration, What might be the cause? how  will we modifiy PCB?

0 Kudos
Reply
1 Reply

1,430 Views
igorpadykov
NXP Employee
NXP Employee

Hi Barry

 

1. one can add codes to dcd header or increase voltage in uboot board file

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6sabresd/mx6sabresd.c?h=...

2. calibration may fail due to power supplies voltages, one can check power requirements,

like ripplies in

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

 

Best regards
igor

0 Kudos
Reply