IMX6ULL DDR3 DEBUG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL DDR3 DEBUG

2,540 Views
dibing
Contributor I

Hi,

We designed a monitoring system using IMX6ULL processor and 1GB DDR3 RAM. There is two DDR3 chips with 512MB.

But, the first DDR chip with chip select 0 (CS0) is neither good nor working properly.

If we are removing the Bad DDR chip1, then can we use the second DDR chip with CS0 by shorting DRAM_CS0 and DRAM_CS1 ?

Labels (3)
Tags (2)
0 Kudos
Reply
2 Replies

2,349 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dibin

shorting DRAM_CS0 and DRAM_CS1 is not allowed, in general one can try to debug

it with jtag (write/read to ddr memory locations and checking waveforms with oscilloscope)

using scripts from ddr test package

i.MX6/7 DDR Stress Test Tool V3.00 

Other options may be running ddr test in lower frequencies and checking power supplies

ripples, should be < 5% as described in Hardware Development Guide for the i.MX6ULL
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,349 Views
dibing
Contributor I

Thanks

0 Kudos
Reply