IMX6ULL DDR3 DEBUG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL DDR3 DEBUG

1,183件の閲覧回数
dibing
Contributor I

Hi,

We designed a monitoring system using IMX6ULL processor and 1GB DDR3 RAM. There is two DDR3 chips with 512MB.

But, the first DDR chip with chip select 0 (CS0) is neither good nor working properly.

If we are removing the Bad DDR chip1, then can we use the second DDR chip with CS0 by shorting DRAM_CS0 and DRAM_CS1 ?

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

993件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dibin

shorting DRAM_CS0 and DRAM_CS1 is not allowed, in general one can try to debug

it with jtag (write/read to ddr memory locations and checking waveforms with oscilloscope)

using scripts from ddr test package

i.MX6/7 DDR Stress Test Tool V3.00 

Other options may be running ddr test in lower frequencies and checking power supplies

ripples, should be < 5% as described in Hardware Development Guide for the i.MX6ULL
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

993件の閲覧回数
dibing
Contributor I

Thanks

0 件の賞賛
返信