IMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL

2,245件の閲覧回数
kerkchoonhuei
Contributor I

Using I.MX6UL, is it possible to use 128MB parallel NOR flash with 2 ENET?

Some of the ENET control pins such RX_ER & RX_EN conflicts with the EXTI pins, does the ENET requires all the pins to be connected accordingly?

What is the minimal required pins that the ENET needs to be connected to function properly?

ラベル(1)
0 件の賞賛
返信
1 返信

1,321件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  You are right, the ENET control pins RX_ER & RX_EN conflict with high EIM address lines.

This does not allow to use both ENET and EIM NOR (128 M). There are no options on i.MX6UL

to resolve such conflict.

Generally, when configuring GPIO, the Processor Expert for i.MX may be useful.

http://www.nxp.com/products/software-and-tools/software-development-tools/processor-expert-and-embed...

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信