Hello,
Background: What I'm trying to do is to add an additional SGTL5000 codec to my own motherboard PCB in additional to the one that already is present on my SOM board.
- The one on the SOM works fine by itself (Connected to SAI1 and I2C2)
The canges I've made so far are the following:
- Added an additional SGTL5000 on my board to SAI2 & I2C4
- The connections are exactly the same as for the one on the SOM
- Made changes to the DTS
- Made changes to a patch file that I think enables the MCLK
The DTS file (Changes in Red):
sound {
compatible = "fsl,imx-audio-sgtl5000";
model = "imx6ul-sgtl5000";
audio-cpu = <&sai1>;
audio-codec = <&codec>;
audio-routing =
"LINE_IN", "Line In Jack",
"MIC_IN", "Mic Jack",
"Mic Jack", "Mic Bias",
"Headphone Jack", "HP_OUT";
};
sound2 {
compatible = "fsl,imx-audio-sgtl5000";
model = "imx6ul-sgtl5000";
audio-cpu = <&sai2>;
audio-codec = <&codec2>;
audio-routing =
"LINE_IN", "Line In Jack",
"MIC_IN", "Mic Jack",
"Mic Jack", "Mic Bias",
"Headphone Jack", "HP_OUT";
};
&clks {
assigned-clocks = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <786432000>;
};
&i2c4 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c4>;
status = "okay";
codec2: sgtl5000@0a {
reg = <0x0a>;
compatible = "fsl,sgtl5000";
clocks = <&clks IMX6UL_CLK_SAI2>;
assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,
<&clks IMX6UL_CLK_SAI2>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <24576000>;
gpr = <&gpr>;
VDDA-supply = <®_3p3v>;
VDDIO-supply = <®_3p3v>;
};
};
&i2c2 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2>;
status = "okay";
codec: sgtl5000@0a {
reg = <0x0a>;
compatible = "fsl,sgtl5000";
clocks = <&clks IMX6UL_CLK_SAI1>;
assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>,
<&clks IMX6UL_CLK_SAI1>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <24576000>;
gpr = <&gpr>;
VDDA-supply = <®_3p3v>;
VDDIO-supply = <®_3p3v>;
};
};
&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog_1>;
imx6ul-nxpu-iopb {
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
MX6UL_PAD_CSI_DATA01__SAI1_MCLK 0x17088 I wonder why this one is here and not in the SAI1grp?
>;
};
pinctrl_i2c1: i2c1grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO02__I2C1_SCL 0x4001b8b0
MX6UL_PAD_GPIO1_IO03__I2C1_SDA 0x4001b8b0
>;
};
pinctrl_i2c2: i2c2grp {
fsl,pins = <
MX6UL_PAD_UART5_TX_DATA__I2C2_SCL 0x4001b8b0
MX6UL_PAD_CSI_VSYNC__I2C2_SDA 0x4001b8b0
>;
};
pinctrl_i2c4: i2c4grp {
fsl,pins = <
MX6UL_PAD_ENET2_TX_DATA0__I2C4_SDA 0x4001b8b0
MX6UL_PAD_ENET2_RX_EN__I2C4_SCL 0x4001b8b0
>;
};
pinctrl_sai1: sai1grp {
fsl,pins = <
MX6UL_PAD_CSI_DATA07__SAI1_TX_DATA 0x17088
MX6UL_PAD_CSI_DATA06__SAI1_RX_DATA 0x17088
MX6UL_PAD_CSI_DATA05__SAI1_TX_BCLK 0x17088
MX6UL_PAD_CSI_DATA04__SAI1_TX_SYNC 0x17088
>;
};
pinctrl_sai2: sai2grp {
fsl,pins = <
MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK 0x17088
MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC 0x17088
MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA 0x11088 /* 120b0 */
MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA 0x11088 /* 130b0 */
MX6UL_PAD_JTAG_TMS__SAI2_MCLK 0x17088
>;
};
&sai1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
status = "okay";
};
&sai2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai2>;
status = "okay";
};
Part of the Patch file:
diff --git a/sound/soc/Makefile b/sound/soc/Makefile
index 974ba70..63302d2 100644
--- a/sound/soc/Makefile
+++ b/sound/soc/Makefile
@@ -10,7 +10,6 @@ snd-soc-core-objs += soc-ac97.o
endif
obj-$(CONFIG_SND_SOC) += snd-soc-core.o
-obj-$(CONFIG_SND_SOC) += codecs/
obj-$(CONFIG_SND_SOC) += generic/
obj-$(CONFIG_SND_SOC) += adi/
obj-$(CONFIG_SND_SOC) += atmel/
@@ -38,3 +37,4 @@ obj-$(CONFIG_SND_SOC) += tegra/
obj-$(CONFIG_SND_SOC) += txx9/
obj-$(CONFIG_SND_SOC) += ux500/
obj-$(CONFIG_SND_SOC) += xtensa/
+obj-$(CONFIG_SND_SOC) += codecs/
diff --git a/sound/soc/codecs/sgtl5000.c b/sound/soc/codecs/sgtl5000.c
index 3a29c0a..e1d582a 100644
--- a/sound/soc/codecs/sgtl5000.c
+++ b/sound/soc/codecs/sgtl5000.c
@@ -29,6 +29,7 @@
#include <sound/soc.h>
#include <sound/soc-dapm.h>
#include <sound/initval.h>
+#include <linux/mfd/syscon.h>
#include "sgtl5000.h"
@@ -1428,11 +1429,14 @@ static int sgtl5000_fill_defaults(struct sgtl5000_priv *sgtl5000)
static int sgtl5000_i2c_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
+ struct device_node *gpr_np;
+ struct regmap *gpr;
struct sgtl5000_priv *sgtl5000;
int ret, reg, rev;
struct device_node *np = client->dev.of_node;
u32 value;
+
sgtl5000 = devm_kzalloc(&client->dev, sizeof(*sgtl5000), GFP_KERNEL);
if (!sgtl5000)
return -ENOMEM;
@@ -1458,6 +1462,18 @@ static int sgtl5000_i2c_probe(struct i2c_client *client,
if (ret)
return ret;
+ gpr_np = of_parse_phandle(client->dev.of_node, "gpr", 0);
+ if (gpr_np) {
+ gpr = syscon_node_to_regmap(gpr_np);
+ if (IS_ERR(gpr)) {
+ ret = PTR_ERR(gpr);
+ dev_err(&client->dev, "failed to get gpr regmap\n");
+ return ret;
+ }
+ /* set SAI1_MCLK_DIR to enable codec MCLK for imx6ul */
+ regmap_update_bits(gpr, 4, 1<<19, 1<<19);
+ regmap_update_bits(gpr, 4, 1<<20, 1<<20);
+ }
+
/* Need 8 clocks before I2C accesses */
udelay(1);
- I assume that the regmap_update_bits(gpr, 4, 1<<20, 1<<20); needs to be done here in order to set the direction for the SAI2 MCLK also?
The error I get when booting linux is:
fsl-asrc 2034000.asrc: driver registered
imx-sgtl5000 sound: mux-int-port missing or invalid
imx-sgtl5000: probe of sound failed with error -22
imx-sgtl5000 sound2: mux-int-port missing or invalid
imx-sgtl5000: probe of sound2 failed with error -22
sgtl5000 1-000a: sgtl5000 revision 0x11
sgtl5000: probe of 3-000a failed with error -5
and naturally later on:
ALSA device list:
No soundcards found.
This means that now neither one of the Codecs are working.
Could anyone point me in the right direction or enlighten me what I have missed or done wrong?
If only the I2C works and there is no MCLK etc. Should I still be able to see the additional codec with, for example, i2cdetect? Because now I only see the codec connected to i2c2.
Thanks in advance,
Jonas