IMX6UL: /sys/fsl_otp/HW_OCOTP_LOCK is not found in 5.4 kernel
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Unfortunately OTP driver is not supported anymore, it was moved to NVMEM framework.
imx-ocotp.c\nvmem\drivers - linux-imx - i.MX Linux kernel
Hope this helps,
Best regards,
Aldo.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
I was working with i.MX6 and kernel 4.9. There we implemented during the flashing process for new u-boot and kernel we write the public key into OTP_SRK*. So next time the device boots it is secured.
Now I want to do the same for i.MX8MM kernel 5.4... But what I have to read here is really disappointing...
Is that still the case? No change to reactivate the FSL driver? An easy way to program eFuses from the userspace.
Now I have to do it in the u-boot. In my case, it means the device needs at least 2 reboots to be in the secure mode. makes no sense to me ...
It just not the same security level...
Dear NXP,
Please give us back the FSL driver?!
Or at least a patch or a workaround that it is possible to use it again.
Any chance for this?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Aldo,
Thanks for the information!
I am able to read the OCOTP registers through the nvmem interface.
$ hexdump ./sys/bus/platform/drivers/imx_ocotp/21bc000.oco
l/imx-ocotp0/nvmem
0000000 c04f 0032 6f41 ea9b 81d4 4732 0000 7032
0000010 0002 0241 0000 0000 004a 0018 0000 0000
0000020 0080 0000 0000 0000 00ba 0000 0000 0000
0000030 0000 0000 0000 0000 0069 5845 0000 0000
0000040 bada bada bada bada bada bada bada bada
*
0000060 687c 4869 8c6d da7e e74a 08f5 782f 0319
0000070 2e6d bab3 c759 050f 6f6c 2fd2 911f 4b7a
0000080 bada bada bada bada 0000 0000 0000 0000
0000090 0000 0000 bada bada 0000 0000 0000 0000
00000a0 0000 0000 0000 0000 0000 0000 0000 0000
00000b0 0000 0000 0040 0000 0000 0000 0000 0000
00000c0 0000 0000 0000 0000 0000 0000 0000 0000
*
0000200
$
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Glad to see you have it working.
Just wondering if you could share the corresponding part of the Device Tree which allows reading of the i.MXD7 NVRAM MAC address?
Regards,
Geoff
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Geoff,
I didn't make any additional changes to get it working as the nvmem entry was provided by the parent device tree file imx6ul.dtsi
ocotp: ocotp-ctrl@21bc000 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "fsl,imx6ul-ocotp", "syscon";
reg = <0x021bc000 0x4000>;
clocks = <&clks IMX6UL_CLK_OCOTP>;
tempmon_calib: calib@38 {
reg = <0x38 4>;
};
tempmon_temp_grade: temp-grade@20 {
reg = <0x20 4>;
};
cpu_speed_grade: speed-grade@10 {
reg = <0x10 4>;
};
};