IMX6UL query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL query

1,806 Views
ramesh6663
Contributor III

In IMX6UL Nxp evk design, Why AUD_INT (audio interrupt ) signal connected to PMIC interrupt and Processor GPIO?

Is there any specific reason?

We are using dedicated GPIO1 for PMIC INT_B signal and GPIO2 for audio codec interrupt signal.

Thanks & Regards,

Rameshkumar

Labels (1)
0 Kudos
Reply
4 Replies

1,665 Views
ramesh6663
Contributor III

Thanks Igor

0 Kudos
Reply

1,665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rameshkumar

AUD_INT (codec headphone detect signal) and PMIC INT are connected to

procesor gpio for future development, currently they are not used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,665 Views
ramesh6663
Contributor III

Thanks Igor,

  So we will use dedicated GPIO1 for PMIC INT_B signal and GPIO2 for audio codec interrupt signal as per our application.

 

Thanks & Regards,

Rameshkumar

0 Kudos
Reply

1,665 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rameshkumar

 

I believe it would be fine

 

Best regards
igor

0 Kudos
Reply