IMX6UL lpddr2 vs ddr3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6UL lpddr2 vs ddr3

1,615 次查看
ricardoferreira
Contributor II

Hi,

Could anyone tell me if there is any specific configuration in the device tree for a memory LPDDR2 compared with DDR3. For example the device tree "imx6ul-14x14-evk.dtb" is for a board with DDR3. If I want to use LPDDR2 do I need to change something?

Regards

R

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,233 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ricardo

seems not, as all memory type definitions are provided in uboot,

except probably max. frequency as "fsl,max_ddr_freq = <400000000>".

In linux AN5125 sect.Introduction to Device Trees describes that in

sect.4 Memory mapping and addressing

http://cache.nxp.com/files/32bit/doc/app_note/AN5125.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复