Hi Miguel
>Is it possible to use sai + tdm + 2 codecs simultaneously with current linux drivers of SAI?
I am afraid such configuration is not supported in current linux.
In general sai driver supports multiple slots in linux/sound/soc/fsl/fsl_sai.c
fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel
.."slots = sai->slots"..
so one can try to debug it.
Also several codecs should be connected appropriately using sai clocks/data description in
Figure 42-1. I2S/SAI block diagram i.MX6UL Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------