MII Connection problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MII Connection problem

4,262 Views
alessandromaggi
Contributor I

Hi,

I have a custom board(designed by us) based on IMX6 SoloX. This board has (among other) two optical ports 100-FX, realized connecting a micrel KSZ8873FLLI via MII to the SoloX.

The problem is that I found an unexpected electrical level on the MII interface in TX direction. I would like the high level to be 3.3V, but on the oscilloscope I quite often can see a stable level around 2 volts.

So on the TX line I can see 3 different voltage level: 3.3V (expected igh level), 2V (unexpected and unwanted high level), and 0V (low level).

Of course with this condition the port is not working.

My question are:

1) Is it possibile for the SoloX to work with an MII interface with 3.3V as high level ? The reference manual is not very clear on this topic.

2) If yes, how the NVCC_SGMII should be connected ?

3) What can cause this strange 3 level signal ?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

4,067 Views
igorpadykov
NXP Employee
NXP Employee

Hi  Alessandro

one can recheck enet power supplies connections using

i.MX6SX Datasheet Table 110. 19x19 mm Functional Contact Assignments

"Power Group" column
https://www.nxp.com/docs/en/data-sheet/IMX6SXCEC.pdf

Also one can look for layout errors and short circuit between traces.

3.3V is allowable value according to Table 10. Operating Ranges i.MX6SX Datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply