IMX6UL ethernet does work in u-boot but it doesn't with Kernel 4.1.15_2.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL ethernet does work in u-boot but it doesn't with Kernel 4.1.15_2.0.0

1,278 Views
zhangjinfei6688
Contributor II

I use imx6ull-14x14-evk ,in uboot mode, it can ping host through eth0,but when start kernel, it can't ping host.The indicator light for the Ethernet interface is also not on.I refer to the  IMX6UL ethernet does work in u-boot but it doesn't with Kernel 3.14.38 ,But it doesn't solve the problem.

Labels (2)
0 Kudos
Reply
2 Replies

1,183 Views
igorpadykov
NXP Employee
NXP Employee

Hi 小飞 张

what bsp used in the case, one can try Demo Images from i.MX Software | NXP 

i.MX 6UltraLite, i.MX 7Dual/Solo Linux Binary Demo Files

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,183 Views
zhangjinfei6688
Contributor II

hi  igorpadykov,Thanks for your reply

      As you said, I downloaded l4.1.15_2.0.0 - ga_images_mx6ullevk.tar.But with MFGTool, no device Connect is displayed after the uboot is loaded.Unable to update system.If I directly use zImage and DTB in l4.1.15_2.0.0 - ga_images_mx6ullevk. tar, the problem of evaluation board is still not solved, that is, after kernel is started, Ethernet is not used.

Looking forward to your reply!

0 Kudos
Reply