IMX6UL boot configuration Resistors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6UL boot configuration Resistors

1,121 次查看
patrickoreilly
Contributor I

Hi, I am designing a board with the IMX6UL. I will have eMMc flash and an SD card as boot options. I have referred to the SPF-2915 for guidance.

I have connected shunt jumpers to the 2x boot mode pins.

However, I do not have room to fit resistors for the boot configuration pins, and will leave these pins unconnected.

As I am developing only the hardware, I want to ensure the code developers can boot from eMMc or SD, if they can enter the serial downloader, and set the efuses to boot from eMMc or SD card.

Is this approach ok?

标签 (1)
0 项奖励
回复
1 回复

924 次查看
BiyongSUN
NXP Employee
NXP Employee

If you have read the datasheet you will find if the boot mode and boot configuration pins are floating.

It has pull down at reset.

Untitled.png