IMX6UL: Using MfgTools for 5.4.3 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL: Using MfgTools for 5.4.3 kernel

2,118件の閲覧回数
sikumar3
Contributor III

Hi, 

We are using MfgTools(2.7) for flashing images to eMMC and we use 4.1.15 kernel.

We are planning to upgrade from 4.1.15 kernel to 5.4.3-2.0.0 (Yocto Zeus).

Since, OCOTP interface has been modified from char driver to nvmem driver, we are not sure whether the ucl2.xml file used by MfgTools will work with latest kernel images or not.

currently, we are using MfgTools with ucl.xml file to burn the fuses. Do we need to change this file content as well for 5.4.3 kernel?

ucl2.xml snippet contains sysfs entries which are no longer created by latest kernel.

<!-- program SRK_HASH fuse -->
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK0">Program SRK0 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK1">Program SRK1 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK2">Program SRK2 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK3">Program SRK3 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK4">Program SRK4 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd> /sys/fsl_otp/HW_OCOTP_SRK5">Program SRK5 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK6">Program SRK6 </CMD>
<CMD state="Updater" type="push" body="$ echo 0xabcdabcd > /sys/fsl_otp/HW_OCOTP_SRK7">Program SRK7 </CMD>

 

Can you please clarify?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,112件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the old MFG Tool does not support this new  versions of Kernel Download, so you need to migrate to our new Tool, which it is named as UUU  ( universal Update tool) here is the link so you can download it

 

https://github.com/NXPmicro/mfgtools/releases

And here is a small training regarding UUU usage

https://community.nxp.com/t5/Connects-Training-Material/Universal-Update-Utility-UUU-Tool/ta-p/11104...

 

 

0 件の賞賛
返信

2,102件の閲覧回数
sikumar3
Contributor III

Hi,

Thanks for the response!

 

Does the UUU tool has backward compatibility? i.e. can we burn images which has older kernel versions with the same tool?

 

Regards,

Siva

タグ(1)
0 件の賞賛
返信

2,090件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is backward compatible.

 

0 件の賞賛
返信