IMX6UL USB_OTG1 Boot Disable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL USB_OTG1 Boot Disable

2,296 Views
renedebacker
Contributor I

I am designing a custom imx6ul board that is configured to boot from eMMC - uSDHC2.  Is there a way to disable booting from the usb_otg1 port if the eMMC boot fails?  We would still need the serial boot functionality for development and production.  I did not see any efuses that disabled usb port serial downloading.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,152 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rene

I am afraid this is not possible, available only fuse SDP_DISABLE

"Disable serial download support" described in Table 5-9. Fusemap Descriptions

Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,152 Views
renedebacker
Contributor I

Igor,

SO setting the Disable Serial Download Support disables USB_OTG1 and UART1/2 downloads?

Regards,

Rene

Rene DeBacker

Hardware Engineering

E: [email protected]<mailto:[email protected]>

O: +1 (830) 980-9782 x1377

Enterprise encryption & key management solutions for

securing the world’s most sensitive data.

0 Kudos
Reply

2,152 Views
igorpadykov
NXP Employee
NXP Employee

yes

Best regards
igor

0 Kudos
Reply