IMX6UL USB_OTG1 Boot Disable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL USB_OTG1 Boot Disable

2,265件の閲覧回数
renedebacker
Contributor I

I am designing a custom imx6ul board that is configured to boot from eMMC - uSDHC2.  Is there a way to disable booting from the usb_otg1 port if the eMMC boot fails?  We would still need the serial boot functionality for development and production.  I did not see any efuses that disabled usb port serial downloading.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,121件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rene

I am afraid this is not possible, available only fuse SDP_DISABLE

"Disable serial download support" described in Table 5-9. Fusemap Descriptions

Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,121件の閲覧回数
renedebacker
Contributor I

Igor,

SO setting the Disable Serial Download Support disables USB_OTG1 and UART1/2 downloads?

Regards,

Rene

Rene DeBacker

Hardware Engineering

E: [email protected]<mailto:[email protected]>

O: +1 (830) 980-9782 x1377

Enterprise encryption & key management solutions for

securing the world’s most sensitive data.

0 件の賞賛
返信

2,121件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

yes

Best regards
igor

0 件の賞賛
返信