IMX6UL Startup problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL Startup problem

2,541 Views
jack_huang1
Contributor IV

Dear,

         I am using the IMX6UL scheme, using BSP L4.1.15_2.0.0, and have now entered the boot. After changing the mfgtools configuration file ucl2.xml, burn the mfgtool2-yocto-mx6ul-evk-nand.vbs card in the starting kernel...  As shown in Figure 1.

        The configuration of ucl2.xml is shown in Figure 2.

         Mfgtools burning log: MfgTool.log, see attachment .

         May I ask: Is the problem with loading the kernel caused by incorrect kernel compilation or device tree issues?

        Thank you!

        Best Regards!

         Jack

0 Kudos
Reply
1 Reply

2,500 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jack_huang1 ,

I hope you're doing well! 

Is there a particular reason to be using an old BSP? Also, I'd recommend using UUU (Universal Update Utility) instead of mfgtools. Let me know if this is of any help.

Thank you.

Best regards,
Hector,

0 Kudos
Reply