IMX6UL Startup problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6UL Startup problem

2,533 次查看
jack_huang1
Contributor IV

Dear,

         I am using the IMX6UL scheme, using BSP L4.1.15_2.0.0, and have now entered the boot. After changing the mfgtools configuration file ucl2.xml, burn the mfgtool2-yocto-mx6ul-evk-nand.vbs card in the starting kernel...  As shown in Figure 1.

        The configuration of ucl2.xml is shown in Figure 2.

         Mfgtools burning log: MfgTool.log, see attachment .

         May I ask: Is the problem with loading the kernel caused by incorrect kernel compilation or device tree issues?

        Thank you!

        Best Regards!

         Jack

0 项奖励
回复
1 回复

2,492 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jack_huang1 ,

I hope you're doing well! 

Is there a particular reason to be using an old BSP? Also, I'd recommend using UUU (Universal Update Utility) instead of mfgtools. Let me know if this is of any help.

Thank you.

Best regards,
Hector,

0 项奖励
回复