IMX6UL Startup problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6UL Startup problem

2,517件の閲覧回数
jack_huang1
Contributor IV

Dear,

         I am using the IMX6UL scheme, using BSP L4.1.15_2.0.0, and have now entered the boot. After changing the mfgtools configuration file ucl2.xml, burn the mfgtool2-yocto-mx6ul-evk-nand.vbs card in the starting kernel...  As shown in Figure 1.

        The configuration of ucl2.xml is shown in Figure 2.

         Mfgtools burning log: MfgTool.log, see attachment .

         May I ask: Is the problem with loading the kernel caused by incorrect kernel compilation or device tree issues?

        Thank you!

        Best Regards!

         Jack

0 件の賞賛
返信
1 返信

2,476件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jack_huang1 ,

I hope you're doing well! 

Is there a particular reason to be using an old BSP? Also, I'd recommend using UUU (Universal Update Utility) instead of mfgtools. Let me know if this is of any help.

Thank you.

Best regards,
Hector,

0 件の賞賛
返信